メインコンテンツに移動

IDT Unveils Wireless Sensor Hub Evaluation Kit for IoT, Smart Home and Other Applications Requiring Real-Time Sensor Data

The IDT® Sensor Module provides critical real-time humidity, temperature and flow data displayed wirelessly on Smartphones and other mobile devices.

2018年1月11日

SAN JOSE, Calif., January 11, 2018 – Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) today introduced its new SDAWIR0x wireless sensor hub evaluation kit, which allows product designers and engineers to validate the advantages of wirelessly connecting IDT’s high-performance humidity, temperature and flow sensors in their latest industrial IoT, smart home, connected appliances, fluid metering and control and environmental monitoring applications. 

The SDAWIR0x development environment integrates IDT’s HS3001 humidity and temperature sensor, FS2012 flow sensor and ZWIR4512 6LoWPAN module and network stack in a single sensor module. The ZWIR4512 connects the environmental sensors via Wi-Fi to output the sensor data in real-time to a private network where it can be viewed on iOS or Android devices.  Up to one hundred of these sensor modules can be connected to a single Wi-Fi hub; or thousands in a full mesh network. Over-The-Air (OTA) firmware updates simplify development and system updates after deployment. This flexible platform makes the SDAWIR0x ideal for a wide variety of connected devices requiring real-time temperature, humidity and flow data, such as smart thermostats, smart refrigerators, environmental weather stations, pumps and metering equipment and medical infusion pumps and CPAPs*.

“The SDAWIR0x uniquely combines our 6LoWPAN solution – which is already proven in smart home and municipal lighting networks – with our royalty-free security stack and OTA update capabilities to provide engineers an industrial-strength development platform for a wide range of IoT, connected home, smart appliance and other applications,” said Sailesh Chittipeddi, IDT’s executive vice president for global operations and chief technology officer.

Wirelessly updating the SDAWIR0x’s firmware is simple and straightforward thanks to the device’s OTA update capability. This includes integrity checking and failure recovery mechanisms to ensure it will not become unusable even in case of error.

The SDAWIR0x security stack enables secure, end-to-end communication – even over unsecure network nodes – with its standard-compliant implementations of the Internet Protocol Security (IPSec) protocol suite and the Internet Key Exchange Protocol version 2 (IKEv2).

IDT’s SDAWIR01 and SDAWIR02 wireless sensor hub evaluation kits are available today worldwide. Visit idt.com/sensorhub to learn more and place orders, or contact your local IDT sales representative.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power, and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

* The IDT SDAWIR0x has not been tested nor certified by the U.S. Food and Drug Administration or other international regulatory authority for use in medical devices.

© 2018, Integrated Device Technology, Inc. IDT  and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする