メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

Imec and Renesas Electronics report record ADC for next-generation high-bandwidth wireless receivers

This world-first 11bit 250MSamples/s SAR ADC achieves a record low-power consumption of only 1.7mWatt

2012年2月23日

Leuven, Belgium and Tokyo, Japan, February 22, 2012 — At this week's International Solid-State Circuit Conference (ISSCC2012), imec and Renesas Electronics Corporation (TSE: 6723) report an innovative SAR (successive-approximation register) ADC (analog to digital converter) with a spectacular improvement in power efficiency and speed, targeting wireless receivers for next-generation high-bandwidth standards such as LTE-advanced and the emerging generation of Wi-Fi (IEEE802.11ac).

SAR ADCs provide high power efficiencies as well as a small form factor, making this architecture attractive for a wide variety of wireless applications. SAR ADCs are frequently the preferred architecture for applications with moderate resolution and sampling frequencies. However, wireless receivers for next-generation high bandwidth standards such as LTE-advanced and the new generations of Wi-Fi require much faster ADCs. This new SAR ADC architecture, developed by imec and Renesas Electronics, is an answer to the need for much faster low-power ADCs with small form factor. The reported ADC is an ultra-low power (1.7mWatt) high resolution (11b) fully-dynamic, two-step interleaved pipelined SAR ADC achieving a record power efficiency of 10fJoule per conversion step at a sampling speed as high as 250MSamples/s. This is a spectacular increase of the speed and sampling frequency, which are both an order of magnitude better than state-of-the art available ADC IP blocks.

This result is obtained with a new converter architecture based on prior groundbreaking ADC designs from imec, cleverly exploiting the opportunities of modern advanced CMOS technologies. The design uses completely dynamic circuits, such that the power consumption scales linearly with the sampling frequency, and is implemented with a maximum amount of digital content, leaving the comparator as the only analog building block.

The ADC prototype has been manufactured in 40nm CMOS with a core chip area of 0.066mm². Measurements show a DNL and INL of respectively 0.8/-0.5 and 1.1/-1.5 LSB. The dynamic performance is characterized by 62dB SNDR (10.0 ENOB) at 10MSamples/s, which is maintained up to 9.5 ENOB level for a sampling speed of up to 250MSamples/s. The power consumption is 6.9pJoule per conversion (70µWatt at 10MSamples/s, 1.7mWatt at 250MSamples/s), resulting in a spectacular energy efficiency of 7 to 10fJoule per conversion-step.

Also at ISSCC, imec and Renesas Electronics present a new way to connect the ADC architecture with the complete radio architecture. To improve the power efficiency of the total receiver system, and avoid issues related to large input capacitors in a voltage-domain ADC system, a 3.2-51.2mSiemens current domain variable-gain transconductor (VGA) was used to drive a charge-domain SAR ADC with no overhead, and as such minimize the overall system power consumption. A 10b 10-80MSamples/s VGA-ADC prototype in 40nm CMOS achieves 70dB DR while consuming less than 5.45mA from a 1.1V supply.

About imec

Imec performs world-leading research in nanoelectronics. Imec leverages its scientific knowledge with the innovative power of its global partnerships in ICT, healthcare and energy. Imec delivers industry-relevant technology solutions. In a unique high-tech environment, its international top talent is committed to providing the building blocks for a better life in a sustainable society. Imec is headquartered in Leuven, Belgium, and has offices in Belgium, the Netherlands, Taiwan, US, China, India and Japan. Its staff of about 1,900 people includes more than 500 industrial residents and guest researchers. In 2010, imec's revenue (P&L) was 285 million euro. Further information on imec can be found at www.imec.be.

Imec is a registered trademark for the activities of IMEC International (a legal entity set up under Belgian law as a “stichting van openbaar nut”), imec Belgium (IMEC vzw supported by the Flemish Government), imec the Netherlands (Stichting IMEC Nederland, part of Holst Centre which is supported by the Dutch Government), imec Taiwan (IMEC Taiwan Co.) and imec China (IMEC Microelectronics (Shangai) Co. Ltd.) and imec India (Imec India Private Limited).

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) Imec is a registered trademark for the activities of IMEC International (a legal entity set up under Belgian law as a “stichting van openbaar nut”), imec Belgium (IMEC vzw supported by the Flemish Government), imec the Netherlands (Stichting IMEC Nederland, part of Holst Centre which is supported by the Dutch Government), imec Taiwan (IMEC Taiwan Co.) and imec China (IMEC Microelectronics (Shangai) Co. Ltd.). All product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.