メインコンテンツに移動

Renesas Electronics Delivers USB Power Delivery Controller Supporting USB Power Delivery 3.0

Revolutionary DC Power Supply with Safe and Secure Power Delivery Technology that Implements Power Supply and Data Communications Over a Single USB Cable

2016年4月13日

TOKYO, Japan, April 13, 2016 — Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the Universal Serial Bus (USB) Power Delivery (PD) controller (part number R9A02G011, successor of µPD720250) that supports USB PD 3.0 specification. The new USB PD controller supports not only PC and smart phone applications, but also a wide range of devices using direct current (DC) power, including PC peripherals, AC adapters, projectors, robots and other consumer electronics.

The USB PD 3.0 specification from USB Implementers Forum (USB-IF) increases the maximum rating of USB charging from 7.5 W (based on the earlier USB specifications) to 100W with different voltage levels up to 20V at 5A. With the arrival of USB PD and the new USB Type-C™ connector, the usage models of USB charging and data communication are expected to increase significantly. The USB PD 3.0 specification adds features such as enabling authentication message exchange for USB Type-C to USB Type-C cables. For device designers and system developers, adopting the Renesas R9A02G011 controller in their devices will make it possible to develop systems with faster charging times. In addition, the new controller reduces system development costs by simultaneously supporting data communication and power supply over a single USB cable, and simplifying many connections existing between devices.

With the rapid demand growth for devices using USB charging, the potential for sub-standard and non-compliant USB accessories (e.g., cables) entering the market increases substantially. The need for identifying non-compliant USB products becomes critically important, particularly for the high-power charging designs based on the USB PD. As a long-time, key supporter of USB-IF, Renesas supports the requirements of the new USB PD 3.0 specification.

Renesas will also deliver R9A02G011-based solutions combining Renesas’ authentication microcontroller (MCU) and advanced power supply control technologies. These solutions will be the building blocks to support the safety, security, efficiency and robustness needs for the upcoming USB PD eco-systems.

Key features of the new USB PD controller and reference boards:

(1) R9A02G011 USB PD controller supporting USB PD 3.0

The R9A02G011 supports both USB PD 3.0 and the USB Type-C specifications. This new device includes integrated on-chip flash ROM, oscillator and power-on reset circuits, and other features, allowing the number of external components to be reduced significantly. As a result, the new USB PD controller can be used in a wide range of applications with limited board space. The R9A02G011 contributes to safe and secure structures in USB PD power supply, supporting systems as well as reduced development costs. It is provided in a small 32-pin QFN package (other package products are under consideration.)

(2) USB PD reference boards that shorten development time and simplify design

In combination with Renesas' power supply technology, Renesas intends to provide an extensive lineup of reference boards that makes manufacturers' design processes even safer and easier. As with the reference boards for the earlier Renesas µPD720250, Renesas will provide an extensive lineup of power-receiving and power-supplying boards that include the new USB PD 3.0 controller. All reference boards make it possible to quickly evaluate the user's existing devices as USB PD supporting devices. By collaborating with other companies, Renesas will provide reference boards as safe and secure solutions, including cables and connectors as well as electronic components.

Availability

Samples of the R9A02G011 are now available. Mass production is scheduled to begin in May 2016 and is expected to reach a volume of 1,000,000 units per month. In addition, Renesas has already started releasing multiple reference boards incorporating this new device. (Availability is subject to change without notice.)

Refer to the separate sheet (PDF: 66 KB) for specifications of the R9A02G011.

For more information on the R9A02G011, please visit: https://www.renesas.com/en/products/renesas-usb-power-delivery-family/c30-group/r9a02g011.html

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) USB Type-C™ and USB-C™ are trademarks of USB Implementers Forum. This product uses SuperFlash® technology licensed from Silicon Storage Technology, Inc. SuperFlash is a registered trademark of Silicon Storage Technology, Inc. in several countries including the United States and Japan. All trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする