メインコンテンツに移動

Portable Washing Machine

2023年3月28日

This Application Note video shows the working Portable Washing Machine. The device is created using the HVPAK SLG47105 as a control module to drive a 12 V DC-DC Motor. In addition, the device has three timer modes, a constant number of revolutions per minute regardless of the load, and under-voltage protection with indication.

Related resources: