メインコンテンツに移動

R-Car S4 SDK: CAN Routing Sample App Part 2

2023-08-03

Renesas provides the R-Car S4 SDK, software that runs on the R-Car S4 SoC.

This video explains the following parts of the procedure for running the CAN routing sample application on the MCAL software for G4MH core.

  • Setting system for executing CAN Routing Sample App
  • Execute CAN Routing Sample App