メインコンテンツに移動

R-Car S4 SDK: Linux BSP Setup App Part 2

2023-08-03

Renesas provides the R-Car S4 SDK, software that runs on the R-Car S4 SoC.

This video, Part 2 of Linux BSP setup in the 'R-Car S4 Startup Guide', explains 'Boot Kernel with TFTP and NFS Server' as the following steps.

  • Set up TFTP and NFS environment then prepare image, DTB files, and userland.
  • Boot up Kernel on Spider board by using TFTP and NFS server.