メインコンテンツに移動

R-Car S4 SDK: Linux BSP UART Sample App Part 1

2023-08-03

Renesas provides the R-Car S4 SDK, software that runs on the R-Car S4 SoC.

This video, Part 1 of Linux BSP setup in the 'R-Car S4 Startup Guide', explains 'System Overview and Sample QSPI, GPIO drivers' as the following steps.

  • Introduce software structure of Linux BSP.
  • Build BSP Image using Yocto Recipe.
  • Introduce operation of QSPI driver.
  • Build and run sample application of GPIO.