メインコンテンツに移動

RA0E1 Fast Prototyping Board Demo

2024年11月14日

This video demonstrates the RA0E1 fast prototyping board, designed for the RA0E1 MCU. It includes a built-in SEGGER J-Link emulator circuit, enabling program writing and debugging without additional tools. The board also provides Arduino UNO and Pmod™ interfaces, along with through-hole access to all microcontroller pins for enhanced expandability.

Chapter's Titles

00:00 Opening
00:40 Unboxing
01:08 Board explanation
01:50 How-to demonstration: E2 Studio
03:55 Example project bundle
04:40 Closing