概要
説明
The RoX (R-Car Open Access) Whitebox is a generic platform to accelerate development using R-Car S4 SoCs and the new generation of R-Car SoCs. The RoX Whitebox stack is built based on OSS including open-source OS and hypervisor that accelerates the development of ADAS, cockpit, and connected services applications. Also, it includes reference applications to jumpstart evaluation and development. All software is provided as an all-in-one package under a Free of Charge (FoC) license, which facilitates testing and can be widely used in advanced development. The open-source based software enables users to freely modify the source code to customize it for their development. Users can also leverage software solutions provided by the Renesas Partner Program.
ソフトウェア一覧
| R-Car S4 Whitebox SDK R-Car S4 Whitebox SDKはコネクテッドサービスのアプリケーション開発を加速させる統合開発プラットフォームです。全てのソフトウェアはFoC (Free of Charge)ライセンスでall-in-one packageとして提供されます。 | Software Package | ルネサス |
1件 | ||
ニュース&ブログ
ブログ 2025年12月18日 |
ニュース 2024年6月20日 |