The Art of Networking (Series 4): CAN XL and 10BASE-T1S – Dataline Performance of Two New Actors in the Networking Arena
This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.
This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.
ルネサスが2020年後半にFSoEソリューションを発売して以来、このソリューションは世界中から注目されています。このブログでは、ルネサスのFSoEソリューションがどのように開発を容易にし、且つ開発期間を短縮するのかをご紹介します。
The Renesas RTD120D two-channel silicon-based thermopile can support healthy air in Canadian classrooms.
“ルネサスの戦略と幅広い車載ソリューションラインナップをアップデートさせていただく機会として「Renesas Automotive Daysオンライン」を開催します。
Wi-Fi 6, the next generation of wireless technology, offers higher speeds and improves signal reliability, network capacity and efficiency in dense deployments.
家電や産業機器の進化・IoT化に貢献してきたRX600シリーズに新製品RX671が加わりました。演算能力・機能が強化されたRX671の追加で、より幅広いニーズへの対応が可能となりました。
ルネサスはアプリケーション処理と標準的なEtherCAT通信、モータ制御をワンチップで実現するRX72M モータ+EtherCAT シングルチップソリューションをご提案します。
This blog provides an overview of the Ka Satcom band LNA lab demo that achieved a new performance benchmark for active beamforming ICs in electronically steered phased array antennas with two simultaneous beams.
Renesas’ Lab on the Cloud bridges the gap between ordering evaluation boards and testing in the lab by providing access to live boards in a physical lab through an online interface.
ソフトウェアによる仮想化はECU統合の用途において強力なツールの1つです。本稿では、2つの仮想マシン間でデータを共有するケースにおいて、①ソフトウェアのみで実現した場合と、②仮想化支援機能を持つ車載イーサネットスイッチを用いた場合について、その比較結果を示します。仮想化を支援する周辺機能(ハードウェア)は、仮想化に伴うオーバーヘッドの低減に貢献します。