The IDE for Gadget Renesas (IDE for GR) is the development environment that enables programming offline. You can use development environments like the Arduino IDE and import a sample, compile, write a program, and debug via a serial monitor.
Supported Boards
The following Gadget Renesas boards are supported by the current IDE for GR version:

Download IDE for GR
Version 1.14
IDE for GR 1.14 for Windows (ZIP) (539MB)
Update Information:
- Updated June 20, 2022
- Related to GR-ADZUKI, GR-COTTON, GR-KURUMI, fixed the problem of compilation with EEPROM.
- Related to GR-SAKURA, GR-CITRUS, fixed the problem with double and float calculation.
- Related to GR-ROSE, add the compile option gnu++11.
Version 1.13
IDE for GR 1.13 for Windows
(ZIP) (538MB)
IDE for GR 1.13 for Mac
(ZIP) (509MB)
Update Information:
- Updated September 2, 2020
- Related to GR-ADZUKI, GR-COTTON, GR-KURUMI, fixed the problem of Serial class, that ignored the settings for configuration like bit width and parity.
Version 1.12
IDE for GR 1.12 for Windows
(ZIP) (538MB)
IDE for GR 1.12 for Mac
(ZIP) (509MB)
Update Information:
- Updated March 12, 2020
- Related to GR-SAKURA, fixed the problem of degrading at V1.11 for using double and float.
- Related to GR-ROSE, updated Wire and Serial libraries.
Version 1.11
IDE for GR 1.11 for Windows
(ZIP) (538MB)
IDE for GR 1.11 for Mac
(ZIP) (509MB)
Update Information:
- Updated December 13, 2019
- Related to GR-ROSE, supported XRCE-DDS-Client via Wi-Fi.
- Related to GR-SAKURA and GR-CITRUS, updated MsTimers and added libraries for networking and MP3 player.
- Related to GR-LYCHEE and GR-PEACH, updated GCC ARM to Version 6 2017.
Version 1.10
IDE for GR 1.10 for Windows
(ZIP) (534MB)
IDE for GR 1.10 for Mac
(ZIP) (391MB)
Update Information:
- Updated September 20, 2019 (*The files that were uploaded on September 19 have been replaced by the above files)
- Related to GR-ROSE, updated XRCE-DDS-Client for ROS2 Dashing Diademata. And updated FreeRTOS from V1.4.6 to V1.4.7
- Related to GR-PEACH, fixed the bug of ArduinoSD library not running correctly
Version 1.09
IDE for GR 1.09 for Windows
(ZIP) (528MB)
IDE for GR 1.09 for Mac
(ZIP) (384MB)
Update Information:
- Updated July 9, 2019
- Related to GR-ROSE, added standard message types for ROS2. Fixed the problem that behavior of Ether.begin became unstable. Fixed a library that handles dynamic memory such as malloc and String. Added web access related libraries such as ArduinoJson, Parser for HTTP, Pub/Sub Client, etc. Other minor corrections were done.
Version 1.08
IDE for GR 1.08 for Windows
(ZIP) (527MB)
IDE for GR 1.08 for Mac
(ZIP) (385MB)
Update Information:
- Updated June 27, 2019
- Fixed the problem that communication failure occurred in WiFiEsp library in GR-ROSE. Other minor corrections were done
Version 1.07
IDE for GR 1.07 for Windows
(ZIP) (527MB)
IDE for GR 1.07 for Mac
(ZIP) (383MB)
Update Information:
- Updated June 21, 2019
- Fixed the problem that MAC address was not set correctly when using Ethernet with GR-ROSE
Version 1.06
IDE for GR 1.06 for Windows
(ZIP) (527MB)
IDE for GR 1.06 for Mac
(ZIP) (384MB)
Update Information:
- Updated May 28, 2019 for Windows/Mac
- Added GR-ROSE board
Version 1.05
IDE for GR 1.05 for Windows
(ZIP) (531MB)
ide-for-gr-v1.05.dmg
(ZIP) (370MB)
Update Information:
- Updated Nov. 21, 2018 for Windows/Mac
- Fixed problem where line numbers are not displayed correctly when scrolling screen
- Fixed problem where a sketch using OpenCV could not be built with GR-PEACH
Version 1.04
IDE for GR 1.04 for Windows
(ZIP) (526MB)
ide-for-gr-v1.04.dmg
(ZIP) (375MB)
Update Information:
- Updated Nov. 1, 2018 for Windows/Mac
- Fixed problem of CPU utilization rate increasing (bug created with v1.03 line indication)
- The following versions of the library were applied:
- GR-PEACH v2.04, GR-LYCHEE v1.04, GR-CITRUS/GR-SAKURA v2.21, GR-KURUMI other RL78 v2.03
Version 1.03
IDE for GR 1.03 for Windows
(ZIP) (334MB)
ide-for-gr-v1.03.dmg
(ZIP) (353MB)
Update Information:
- Updated Feb 2, 2018 for windows, Feb 8, 2018 for Mac
- Line numbers can now be displayed
- Ensures that "core dependency" error does not appear in Arduino library import
- Updated the library of GR-PEACH to v2.03. Addition of LCD libraries was done
- Updated the library of GR-LYCHEE to v1.02. Addition of LCD libraries was done
Version 1.02
IDE for GR 1.02b for Windows
(ZIP) (337MB)
IDE for GR 1.02 for Mac
(ZIP) (410MB)
Note: The volume label of GR-CITRUS has been changed to "GR-CITRUS_b" by updating the USB mass storage firmware. With v1.02 or less, "GR-CITRUS is not found" is displayed at the time of writing. The Windows version is compatible with v1.02b. The Mac version is compatible with v1.03.
Version 1.01
IDE for GR 1.01 for Windows
(ZIP) (322MB)
ide-for-gr-v1.01.dmg
(ZIP) (393MB)
Version 1.00
IDE for GR 1.00 for Windows
(ZIP) (321MB)
IDE for GR 1.00 for Mac
(ZIP) (325MB)
Installation Notes
Windows
For Windows, it is not in the installation format. After extracting the zip file, please start the exe file.
Mac
For Mac, after mounting the dmg file, move the IDE for GR to the application folder.
Supported Operating Systems
Windows
- Windows 7 32/64-bit
- Windows 8.1 32/64-bit
- Windows 10 32/64-bit
Mac
- OS X 10.9 Mavericks
- OS X 10.10 Yosemite
- OS X 10.11 El Capitan
- OS X 10.12 Sierra (Evaluated on v1.03)
- OS X 10.13 High Sierra (Evaluated on v1.03)
About the Libraries
In IDE for GR, in order to reduce the compilation time, most libraries archive and use compiled objects, and their sources are deleted.
The archive file uses gr_common.a generated by the build of the web compiler, but when changing the library, it is recommended to use an IDE that allows project management such as e2 studio.