メインコンテンツに移動

ブログ

4 Benefits of Solar Power Realized by Smart Solar Battery Charger Solution

4 Benefits of Solar Power Realized by Smart Solar Battery Charger Solution

This blog introduces Renesas' Smart Solar Battery Charger solution.

‘Tried & True’ – Renesas MCUs Are Made for You

確かな信頼を誇る、お客様を第一に考えたルネサスのMCU

デュアルソース生産モデル、業界で最も先進的な MCU プロセス技術、およびエコシステム パートナーの広大なネットワークに裏打ちされたスマートでセキュアな MCU を設計する当社の数十年にわたる経験を活用して、次の設計を簡素化し、迅速に市場に投入する方法をご覧ください。

The I3C Interface Can Help Improve Performance in Sensor Applications

The I3C Interface Can Help Improve Performance in Sensor Applications

Looking at how the I3C bus can help with connectivity problems around connecting multiple sensors to a device as well as providing a performance increase to applications using the I2C bus today.

The Art of Networking

The Art of Networking (Series 11): Power over Data Line in Action

Power over Data Line (PoDL) is ideal for small sensor and actor applications. To support customers, Renesas has prepared a PoDL reference design and tested it for a radar use case.

Low Power Consumption of RX MCU

RXマイコンの低消費電力モード使い分けとコツ

RXマイコンの低消費電力モードへの移行方法や注意事項、ノウハウなどを説明したアプリケーションノートをご紹介します。

Develop The Touch Functions Of RX671 Quickly And Easily

誰でも簡単かつ短期間でタッチ機能を開発!RX671のタッチキーソリューション

評価キット"RX671搭載静電容量タッチ評価システム"と静電容量タッチキーソリューションを用いて、ノウハウが必要なタッチキー機能の開発を誰でも簡単に着手できるようになりました。

Drive without Limits: Interoperable Electric Vehicle (EV) Chargers

限界のない走りを目指して - スマートEV充電器ソリューション

ルネサスは、電気自動車(EV)充電に対応する3KWオフボードEV充電器ソリューションを提供します。

The No-Code Paradigm Shift in Product Firmware Development

Quick-Connect Studio enables rapid firmware development using zero coding methodologies via graphical drag-and-drop of major system solution blocks and automatic firmware generation.

Revving the RISC-V Engine to Help Designers Explore Breakthrough Processor Architecture

Revving the RISC-V Engine to Help Designers Explore Breakthrough Processor Architecture

As RISC-V generates significant interest in the design community, Renesas uses its comprehensive MCU/MPU ecosystem to develop commercially viable solutions that accommodate any development path.