メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

ブログ

Renesas Smallest Touch Microcontroller for 8-Bit MCU Market

ルネサス最小のタッチマイコンが登場

今の製品にタッチ機能を取り入れたいけど、スペースがない…そんな方に、ルネサス最小のタッチマイコンRL78/G16の魅力をお伝えします。また、すぐにRL78/G16をお試しできるお手頃な評価ボードと、タッチ専用の評価システムもご紹介します。

Introducing the Tool to Set Pins of RZ Series Easily for Linux

Introducing the Tool to Set Pins of RZ Series Easily for Linux

Recently MPUs have many functions and the setting of shared pins that assign multiple functions to one pin has become complicated. In addition, the number of pins has increased. So, it became difficult to set pin configurations manually without making mistakes. In this blog, “Smart Configurator for RZ” is introduced for Linux on RZ MPU series.

Market and Technology Trends for EV Charging Stations

EV用充電ステーションの市場動向と技術トレンド

現在、世界中で自動車の電動化(EV化)が急速に進んでいます。一方で、EVが普及するためには、充電ステーションの普及が重要です。本ブログでは、EV用充電ステーションの市場動向と技術トレンドを紹介します。

Reducing Noise Issues in Microcontroller Systems

Reducing Noise Issues in Microcontroller Systems - Part 3

This series of blogs (in three parts) discusses how noise can affect a microcontroller system and provides design ideas on how a microcontroller system can be made more robust in the presence of noise.

Giving a Helping Hand to AC Servo Motors in Robots Blog

Giving a Helping Hand to AC Servo Motors in Robots

Renesas offers a comprehensive AC Servo Kit solution, using the RZ/T2L MPU and features servo control with various communication protocols, as well as field sensors for data collection via remote IO.

Using ECC to Correct Soft Errors on the RA Family

Using ECC to Correct Soft Errors on the RA Family

This blog looks at how we can correct soft errors in the RA microcontroller family SRAM it discusses how soft errors occur, and looks at how our implementation of an error correction function in the SRAM can both detect and correct these errors.

RX Blog: RX66T Digital Power Conversion

RXマイコンによるトーテムポールインターリーブPFCの実現

AC-DC電源制御の例としてRXマイコンによるトーテムポールインターリーブPFCの制御方法を紹介します。

Reducing Noise Issues in Microcontroller Systems

Reducing Noise Issues in Microcontroller Systems - Part 2

This series of blogs (in three parts) discusses how noise can affect a microcontroller system and provides design ideas on how a microcontroller system can be made more robust in the presence of noise.

Free Topology: The Ultimate Wired Architecture for Industrial IoT

Free Topology: The Ultimate Wired Architecture for Industrial IoT

Free Topology (FT) is the most cost-effective, highest-performance solution for industrial wired networks compared to alternatives including RS-485 and Ethernet.

The New RX26T – Ideal Microcontroller for Motor Control Applications

モータ制御アプリケーションに最適な新製品!RX26Tのご紹介

2モータ+PFC制御を1チップで実現できる新RXマイコン RX26Tをご紹介します。